VLSI Commodore AKIKO asic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VLSI Commodore AKIKO asic

2,671件の閲覧回数
cd32freak
Contributor I

Hello,

In 1993 Commodore released a computer called the Amiga CD32. There was a VLSI asic on the motherboard called AKIKO (see https://upload.wikimedia.org/wikipedia/commons/4/41/Amiga-CD32-Motherboard-Top.jpg). In 1999 Philips acquired VLSI Technology Inc., which means they also own the design of the AKIKO. Some users in the small Amiga community want to remake the AKIKO with a FPGA chip, but they need technical information about the AKIKO. Would it be possible to help them out? This is the information on the chip:

VLSI
9340BS
444182
VY06575-2
AKIKO REV AKIKO
CBM 391563-01

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 返信

2,617件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello Kerim,

Unfortunately, we don't have any information available from VLSI products. Please, if you need some additional products to complete your design that we can help you with, let us know and we will be happy to help you.


Have a great day,
Fabian

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

Best Regards,
Fabian
0 件の賞賛
返信