I am running into a problem where the SE050 gives me a conditions of use not satisfied (69 85)
on writing the public key . I think it has to do something with the policy setting .
Can nxp provide me an example apdu sequence of loading an external ecc brainpool public key ?
Because we use the LPC1754 I am not able to use the supplied examples but I had to go my own way .
Hi Rick,
Actually we have any example to prepare the raw APDU commands for that purpose, and because it needs to load a file contain the key value, so the host is based on PC/Linux, and the APDU commands are sent to SE050 via a bridge of USB VCOM to I2C port.this example imports AES key for demo, but you may change it to WriteECKey command.
Please kindly refer to the following for more details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------