S32K1xx Examples can not dowload

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1xx Examples can not dowload

2,417 Views
2529434362
Contributor I

您好,我下载一个例程,然后下载地址是这个,S32K1xx Examples ,去下载的时候,显示里面的附件木有了,附件附件名称是这几个,请问一下怎么回事?谢谢您!

附件1.Example_S32K144-Flash_RW_simple-S32DS12.zip

附件2.Example-S32K144-DMA-RAM2RAM-test-v1_0-S32DS.zip

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,318 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 余 帅,

I can only find the "Example_S32K144-Flash_RW_simple-S32DS12.zip" in who can give me the method of operation about s32k144 flash,such as example of the code and informat....

Would you please refer the DMA example in S32DS.ARM2.2?

edma_transfer_s32k144.png

eDMA Transfer.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply