Mass erase

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mass erase

Jump to solution
4,730 Views
814420552
Contributor III

hello,

    <1>  is the following protected in the red box write protection?

pastedImage_1.png

    <2>  if partition has CSE key sapce but no save any CSE key, then enable security, debugger also  can not remove security?? 

1 Solution
4,664 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Kui Wu,

1. This refers to the Flash protection, please see below the description of Program Flash Protection Registers.

pastedImage_1.png

2. Yes, in this case, it is not possible to mass erase the MCU.

pastedImage_2.png

AN12130 Production Flash Programming Best Practices for S32K1xx MCUs

Regards,

Daniel

View solution in original post

0 Kudos
Reply
4 Replies
4,664 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello  Kui Wu,

If you could provide the name of the NXP product you are using and which document did you extract this information, I will gladly help you with your question.
Have a great day,
Fabian

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

Best Regards,
Fabian
0 Kudos
Reply
4,664 Views
814420552
Contributor III

My device is S32k146UAVLQ and extract this informatio form S32K11X-14X.pdf   chapter 5.2.1.1

thank you!

0 Kudos
Reply
4,665 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Kui Wu,

1. This refers to the Flash protection, please see below the description of Program Flash Protection Registers.

pastedImage_1.png

2. Yes, in this case, it is not possible to mass erase the MCU.

pastedImage_2.png

AN12130 Production Flash Programming Best Practices for S32K1xx MCUs

Regards,

Daniel

0 Kudos
Reply
4,664 Views
814420552
Contributor III

Dear Daniel,

      thanks for your answer in time! I have marked  this answer is right!