MRF101AN-40MHZ Reference Kit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MRF101AN-40MHZ Reference Kit

跳至解决方案
2,101 次查看
davorin_kotnik
Contributor I

I have a kit MRF101AN 40.68 MHz Reference Circuit. Can I power the MRF101AN 40.68 MHz Reference Circuit with a lower voltage of 24V or 28V. I need an output rf power adjustable from 20W to 40W.

0 项奖励
回复
1 解答
2,096 次查看
LPP
NXP Employee
NXP Employee

You can run MRF101AN 40.68 MHz Reference Circuit at low voltage without extra risk of damage.

Estimated output power will be about 31 Watts at 28V.

Have a great day,
Pavel
TIC

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,097 次查看
LPP
NXP Employee
NXP Employee

You can run MRF101AN 40.68 MHz Reference Circuit at low voltage without extra risk of damage.

Estimated output power will be about 31 Watts at 28V.

Have a great day,
Pavel
TIC

 

0 项奖励
回复