MRF101AN-40MHZ Reference Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRF101AN-40MHZ Reference Kit

Jump to solution
2,213 Views
davorin_kotnik
Contributor I

I have a kit MRF101AN 40.68 MHz Reference Circuit. Can I power the MRF101AN 40.68 MHz Reference Circuit with a lower voltage of 24V or 28V. I need an output rf power adjustable from 20W to 40W.

0 Kudos
Reply
1 Solution
2,208 Views
LPP
NXP Employee
NXP Employee

You can run MRF101AN 40.68 MHz Reference Circuit at low voltage without extra risk of damage.

Estimated output power will be about 31 Watts at 28V.

Have a great day,
Pavel
TIC

 

View solution in original post

0 Kudos
Reply
1 Reply
2,208 Views
LPP
NXP Employee
NXP Employee

You can run MRF101AN 40.68 MHz Reference Circuit at low voltage without extra risk of damage.

Estimated output power will be about 31 Watts at 28V.

Have a great day,
Pavel
TIC

 

0 Kudos
Reply