LS1046A with Linux OS FPGA Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A with Linux OS FPGA Driver

2,392件の閲覧回数
trevor_frederic
Contributor I

I have an LS1046A board running Ubuntu, built using flexbuilder, attached to the LS1046 board is a FPGA device via PCIe.  We're writing a driver for the FPGA.  The OS sees the device and we can run ioremap() to map physical to kernel memory which returns a high memory address; however, any attempt to use ioread() results in a kernel crash, and no additional information.  We've looked through all the Linux device driver books/forums and haven't had any luck in finding out what might be going on.

タグ(2)
0 件の賞賛
返信
1 返信

2,346件の閲覧回数
Pavel
NXP Employee
NXP Employee

Check your code using the following pages:

https://www.opensourceforu.com/2011/06/generic-hardware-access-in-linux/

 

https://lwn.net/Articles/102232/

 

https://stackoverflow.com/questions/19100536/what-is-the-use-of-iomem-in-linux-while-writing-device-...

 

https://stackoverflow.com/questions/26831583/ioread32-followed-by-iowrite32-not-giving-same-value

 

https://www.oreilly.com/library/view/linux-device-drivers/0596005903/ch09.html

 

https://01.org/linuxgraphics/gfx-docs/drm/driver-api/device-io.html

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 件の賞賛
返信