LPC540: Voltage at ADC input before VDD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC540: Voltage at ADC input before VDD

1,414件の閲覧回数
jana_beck
Contributor II

Hi,
I have a design, where I am trying to measure voltages with a LPC54016.
One ADC input is a voltage, that will be on an ADC pin, before the MCU gets powered.

I have VCC_5V that gets converted into VCC_3V3 with a step down DCDC converter.
I have 5V going to an ADC input (with a voltage divider, so it is 2.25V at the pin).
That means, that the 2.25V will be on the ADC pin before 3.3V at the power supply pins.

Can this damage the MCU?

Thanks,
Jana

0 件の賞賛
返信
1 返信

1,364件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Jana Beck

 

Due to the internal circuitry, it is not recommendable to apply voltage to the pins before powering the VDD, this may cause you trouble with the MCU.

I apologize for the inconvenience this is causing you, if you have more questions do not hesitate to ask me.

Best regards,

Omar

0 件の賞賛
返信