K32L2A31VLL1A Schematic/Sample Design

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K32L2A31VLL1A Schematic/Sample Design

14,516 次查看
kapil_kesharvan
Contributor I

Hi,

I want to use the "K32L2A31VLL1A" MCU to develop the design for one of my products.  I have gone through the below links.

1. K32L2A31VLL1A Product Information|NXP 

2. https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

I have gone with some of the documents and evaluation boards but I was not able to get the proper design for the MCU. 

Can someone suggest if they have the design for this MCU?

Your support in this regard will be highly appreciable. And Thank you so much in Advance.

Regards

Kapil

0 项奖励
回复
8 回复数

14,399 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Kapil Kesharvani,

    The K32L2A31VLL1A related circuit can refer to the  FRDM-K32L2A4S schematic directly.

    FRDM-K32L2A4S on board chip is K32L2A41VLL1A, your chip is K32L2A31VLL1A , even the package is the same, just the Flash and SRAM difference:

pastedImage_3.png

About the samples, you can apply it from the nxp.com:

 You can find it is active now.

pastedImage_2.png

About the board, you can refer to the FRDM-K32L2A4S, you can use FRDM-K32L2A4S directly or change the on board chip to K32L2A31VLL1A.

About the peripheral hardware, the same as FRDM-K32L2A4S, you can refer to it directly.

1. SPI (1 no.)

pastedImage_4.png

2. I2C (1 no.)

pastedImage_5.png

3. UART(1 no.)

pastedImage_6.png

4. JTAG Debug

pastedImage_7.png

5. GPIOs, (30/40 numbers)

  Check the fanout J1,J2, J3,J4 refer to your own design.

6. Clock, Reset, etc...

 clock, 

pastedImage_8.png

reset pin, 4.7K to 10K pullup, and 0.1uf capacitor to ground.

More details, check the FRDM schematic which I give you, you totally can refer to it.

Wish it helps you!

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

14,395 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Kapil Kesharvani,

  Thanks for your interest in the NXP kinetis product, I would like to provide service for you.

  K32L2A31VLL1A can refer to the FRDM-K32L2A4S:

FRDM-K32L2A4S Platform | Freedom Development Board | K32 L MCUs | NXP 

  But, it seems the design file still not put in the nxp website.

  Anyway, I will help you to check it with our internal side,apply for upload the related schematic and the design file to the website.

  Here I share with you one K32L2A4 schematic at first.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

14,395 次查看
kapil_kesharvan
Contributor I

Hello Kerry,

 

Thank you so much for your reply. 

Since we are going to finalize this MCU. So it is possible to share the sample design/ Application for the same MCU as soon as possible. And we need some samples and evaluation boards. so how soon we can get this?

 

 As mentioned before, I am going through the datasheet and try to understand the features that we are looking for. But for better clarification can you suggest which pins are good for the below features.

The main features that we are going to use are:

1. SPI (1 no.)

2. I2C (1 no.)

3. UART(1 no.)

4. JTAG Debug

5. GPIOs, (30/40 numbers)

6. Clock, Reset, etc...

 

Regards

Kapil

0 项奖励
回复

14,395 次查看
kapil_kesharvan
Contributor I

Hi Kerry,

I am sorry for the late reply. and thank you so much for your inputs.

Let me go through the inputs you shared. I will come back.

Regards

Kapil

0 项奖励
回复

14,395 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Kapil Kesharvani

   You are welcome!

   If you have the question about this case, just let me know.

  If you have the new questions, please create the new question post, thanks.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

14,395 次查看
kapil_kesharvan
Contributor I

Hello Kerry,

Thank you so much for your reply. 

Since we are going to finalize this MCU. So it is possible to share the sample design/ Application for the same MCU as soon as possible. And we need some samples and evaluation boards. so how soon we can get this?

As mentioned before, I am going through the datasheet and try to understand the features that we are looking for. But for better clarification can you suggest which pins are good for the below features.

The main features that we are going to use are:

1. SPI (1 no.)

2. I2C (1 no.)

3. UART(1 no.)

4. JTAG Debug

5. GPIOs, (30/40 numbers)

6. Clock, Reset, etc...

Regards

Kapil

0 项奖励
回复

14,395 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Kapil Kesharvani , 

   Please check the SDK code for FRDM-K32L2A4S from this link:

https://mcuxpresso.nxp.com/en/select

  You will find all the related sample code for the perpherals.

  Wish it helps you!

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

14,395 次查看
kapil_kesharvan
Contributor I

Hi Kerry,

Thanks for the reply. and sharing the inputs. 

But my query was related to Schematic design.

 it is possible to share the MCU (K32L2A31VLL1A) sample design (Circuit)/ Application design.

As mentioned before, I am going through the datasheet and try to understand the features that we are looking for. But for better clarification can you suggest which pins are good for the below features.

The main features that we are going to use are:

1. SPI (1 no.)

2. I2C (1 no.)

3. UART(1 no.)

4. JTAG Debug

5. GPIOs, (30/40 numbers)

6. Clock, Reset, etc...

And we need some samples and evaluation boards. what will be the lead time?

Regards

Kapil

0 项奖励
回复