Help with TDA19988

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help with TDA19988

2,563件の閲覧回数
Popkkka
Contributor I

Hi.

I consider using TDA19988 to design HDMI transmitter circuit.

I wonder thd default setting of input port for RGB888.

Datasheet confuses me.

...
0 件の賞賛
返信
1 返信

2,561件の閲覧回数
elena56brown
Contributor I

I understand that the datasheet can be a bit confusing. For the TDA19988 HDMI transmitter, the default setting for the input port when using RGB888 is typically 24 bits per pixel. This means that each pixel is represented by 24 bits, with 8 bits each for red, green, and blue.

Here are some general steps to configure the TDA19988 for RGB888:

Input Format: Set the input format to RGB888.

Pixel Format: Ensure that the pixel format is set to RGB888.

Resolution: Configure the resolution according to your requirements (e.g., 1920x1080).

Color Depth: Set the color depth to 24 bits per pixel.

0 件の賞賛
返信