Help with TDA19988

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help with TDA19988

2,565 Views
Popkkka
Contributor I

Hi.

I consider using TDA19988 to design HDMI transmitter circuit.

I wonder thd default setting of input port for RGB888.

Datasheet confuses me.

...
0 Kudos
Reply
1 Reply

2,563 Views
elena56brown
Contributor I

I understand that the datasheet can be a bit confusing. For the TDA19988 HDMI transmitter, the default setting for the input port when using RGB888 is typically 24 bits per pixel. This means that each pixel is represented by 24 bits, with 8 bits each for red, green, and blue.

Here are some general steps to configure the TDA19988 for RGB888:

Input Format: Set the input format to RGB888.

Pixel Format: Ensure that the pixel format is set to RGB888.

Resolution: Configure the resolution according to your requirements (e.g., 1920x1080).

Color Depth: Set the color depth to 24 bits per pixel.

0 Kudos
Reply