Help with TDA19988

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help with TDA19988

1,280 次查看
Popkkka
Contributor I

Hi.

I consider using TDA19988 to design HDMI transmitter circuit.

I wonder thd default setting of input port for RGB888.

Datasheet confuses me.

...
0 项奖励
回复
1 回复

1,278 次查看
elena56brown
Contributor I

I understand that the datasheet can be a bit confusing. For the TDA19988 HDMI transmitter, the default setting for the input port when using RGB888 is typically 24 bits per pixel. This means that each pixel is represented by 24 bits, with 8 bits each for red, green, and blue.

Here are some general steps to configure the TDA19988 for RGB888:

Input Format: Set the input format to RGB888.

Pixel Format: Ensure that the pixel format is set to RGB888.

Resolution: Configure the resolution according to your requirements (e.g., 1920x1080).

Color Depth: Set the color depth to 24 bits per pixel.

0 项奖励
回复