Does the JN5169 device support RF4CE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the JN5169 device support RF4CE?

2,985件の閲覧回数
854648943
Contributor III

Hi,

Does the JN5169 device support the rf4ce protocol? 

I went to see the documents related to RF4CE, and it seemed that just supported the documents that supported JN5168.

JN5169 i don't seem to support RF4CE,for this application. Is it possible to support the RF4CE protocol on the board of JN5169

タグ(2)
0 件の賞賛
返信
7 返答(返信)

2,834件の閲覧回数
854648943
Contributor III

Hi,

I added the content of JN5169 to the application template JN-AN-1200-ZigBee-RF4CE-Application-Template, compiled it, downloaded it to my development board, and worked properly, but I found that when I was pairing, I always failed. Did JN5169 not support RF4CE on a hardware basis?

I need your help. thank you.

regardes

han

0 件の賞賛
返信

2,834件の閲覧回数
854648943
Contributor III

NXP Designs‌

Hello,Do JN5169 support RF4CE? 

 I have been waiting for the exact reply, our company needs to customize the program based on the results, i tried is not enough. But i

don't know if there is anything missing in my attempt, so i hope i can get your help.

Regardes

Han

0 件の賞賛
返信

2,834件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Could you please help me check this post ?

zigbee3.0 

Regards,

Estephania

0 件の賞賛
返信

2,835件の閲覧回数
854648943
Contributor III

Hi,Estephania Martinez

Thank you for your reply.

If you look at my question carefully, then you will find that I am not asking if zigbee3.0 supports rf4ce.

My question is whether RF4CE, is supported on JN5169 hardware because I didn't see support for JN5169, in the

RF4CE-related SDK and the introduction, and I tried to modify the compilation options for this

JN-AN-1200-ZigBee-RF4CE-Application-Template, and now I can download the code to JN5169 and run, but there

are always problems when pairing is not successful.

SDK is JN-SW-4060

Regards,

Han

0 件の賞賛
返信

2,835件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

We currently do not have anything of RF4CE as a standalone, only the ones in the ZigBee 3.0, RF4CE  is no longer supported as mentioned in the post I referenced.

I'm sorry for the inconveniences this might cause you.

Regards,

Estephania

0 件の賞賛
返信

2,834件の閲覧回数
854648943
Contributor III

Hi,Estephania Martinez

  

Thank you for your reply.

Sorry, I can' t understand you say :" We currently do not have anything of RF4CE as a standalone, only the ones in the ZigBee 3.0,

RF4CE  is no longer supported as mentioned in the post I referenced"

Is rf4ce no longer supported now, if i use jn5168 to run rf4ce demo properly.

Regards,

Han

0 件の賞賛
返信

2,834件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

The SW in the application note you are using, which correspond to the following link, is the one that is no longer supported.

Sorry, for the inconveniences this might cause you.

Regards ,

Estephania

0 件の賞賛
返信