Build Layerscape LDP image (ls1088ardb-pb) using bitbake (yocto)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build Layerscape LDP image (ls1088ardb-pb) using bitbake (yocto)

2,692 Views
Lini
Contributor I

Hi,

When i build image for ls1088ardb-pb using bitbake i faced below error.
how to solve it


bitbake ls-image-lite

ERROR: linux-qoriq-6.1.y+gitAUTOINC+66e442bc7f-r0 do_assemble_fitimage_initramfs: Could not find a valid initramfs type for core-image-minimal-ls1088ardb-pb, the supported types are: cpio.lz4 cpio.lzo cpio.lzma cpio.xz cpio.zst cpio.gz ext2.gz cpio
ERROR: linux-qoriq-6.1.y+gitAUTOINC+66e442bc7f-r0 do_assemble_fitimage_initramfs: ExecutionError('/home/wilburl/NXP/yocto/build_ls1088ardb-pb/tmp/work/ls1088ardb_pb-fsl-linux/linux-qoriq/6.1.y+gitAUTOINC+66e442bc7f-r0/temp/run.do_assemble_fitimage_initramfs.2619713', 1, None, None)
ERROR: Logfile of failure stored in: /home/wilburl/NXP/yocto/build_ls1088ardb-pb/tmp/work/ls1088ardb_pb-fsl-linux/linux-qoriq/6.1.y+gitAUTOINC+66e442bc7f-r0/temp/log.do_assemble_fitimage_initramfs.2619713
ERROR: Task (/home/wilburl/NXP/yocto/sources/meta-qoriq/recipes-kernel/linux/linux-qoriq_6.1.bb:do_assemble_fitimage_initramfs) failed with exit code '1'

0 Kudos
Reply
2 Replies

2,639 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please apply the attached patches.

0 Kudos
Reply

2,664 Views
Lini
Contributor I

When I build the LDP image for the LS1088ARDB, it works fine. However, when I try to build it for the LS1088ARDB-PB, I encounter an error. Should I make any changes to the conf/local.conf file or the ls-image-lite.bb file to resolve this issue?

0 Kudos
Reply