ARM 64 tiny itb file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ARM 64 tiny itb file

2,067 Views
ranga_yn
Contributor III

Hello NXP,

Does the lsdk_linux_arm64_tiny.itb  is different from LS1088 and LS2088. If different where can I get LS2088 arm64 tiny lib file.

regards,

ranga

Labels (1)
0 Kudos
Reply
1 Reply

1,861 Views
Pavel
NXP Employee
NXP Employee

The lsdk_linux_arm64_tiny.itb includes kernel, .dtb file and root file system for all arm64. it includes the LS1088a and the LS2088a.

This .itb file is built using .its file. See the linux_arm64_LS.its using the following path:

/LSDK_1909/flexbuild_lsdk1909/configs/linux

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply