ARM 64 tiny itb file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ARM 64 tiny itb file

1,979件の閲覧回数
ranga_yn
Contributor III

Hello NXP,

Does the lsdk_linux_arm64_tiny.itb  is different from LS1088 and LS2088. If different where can I get LS2088 arm64 tiny lib file.

regards,

ranga

ラベル(1)
0 件の賞賛
返信
1 返信

1,773件の閲覧回数
Pavel
NXP Employee
NXP Employee

The lsdk_linux_arm64_tiny.itb includes kernel, .dtb file and root file system for all arm64. it includes the LS1088a and the LS2088a.

This .itb file is built using .its file. See the linux_arm64_LS.its using the following path:

/LSDK_1909/flexbuild_lsdk1909/configs/linux

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信