S32G just support serial download a M7 image to run by internal rom codes, our S32G DS IDE have a flash tools to use this feature to burn the image to external device. So current image burn method will divide into 2 step:
1: burn a uboot into the external device by S32G DS flash tools.
2: reboot the codes with uboot and run with network to burn the linux image into external device.
which need two working place on manufacture line, and customer wish to have a one time on-line tools, which means we need use serial port to boot uboot directly but S32G rom codes do not support it.
We have a reference tools of S32V but which IP difference is big between on S32V and S32G, So we can not reuse it and have to develop a new one.
The development working include:
序号
开发工作
说明
开发者
1
开发
根据S32G的serial boot协议要求,开发PC端的串口工具来下载M7镜像
John.Li
2
开发
根据自定义协议要求,开发PC端的串口工具来下载A核Bootloader到SRAM中
John.Li
3
开发
根据自定义协议要求,开发M7镜像的串口接收与Checksum逻辑
John.Li
4
开发
修改M7镜像支持串口0
John.Li
5
开发
开发实现M7镜像的串口单字节同步收发函数
John.Li
6
开发
开发实现A53启动功能
John.Li
7
调试与Debug
调试解决串口接收乱码问题(Serial boot rom codes仍然在回送消息串口)
John.Li
8
调试与Debug
提供 解决A核启动串口halt思路(Serial boot rom codes仍然占用串口)
John.Li
9
调试与Debug
优化M7镜像,缩小大小
Tony.Zhang
10
调试与Debug
根据M7镜像和A核 Uboot在SRAM中的内存分配要求,重排M7镜像位置,避免冲突
Tony.Zhang
11
调试与Debug
在M7中初始化SRAM空间
Tony.Zhang
12
调试与Debug
在M7中设置SRAM可执行空间
Tony.Zhang
13
调试与Debug
调试解决由于cache没有及时回写导致的下载镜像错误的问题
Tony.Zhang
14
调试与Debug
集成,调优与文档
John.Li
Pls check the attachment for the doc/codes/binary release which include:
Release
|->M7: Linflexd_Uart_Ip_Example_S32G274A_M7: S32DS M7工程。
|->PC: s32gSerialBoot_Csharp: PC端的Visual Studio的C#的串口工具工程。
|->Test:
| |-> 115200_bootloader.bin: S32DS M7工程编译出来的bin文件,波特率为115200
| |-> 921600_bootloader.bin: S32DS M7工程编译出来的bin文件,波特率为921600
| |->load_uboot.bat: 运行工具的批处理文件,运行成功后打开串口可以看到Uboot执行,默认使用的波特率是115299
| |->readme.txt:其它测试命令
| |->s32gSerialBoot.exe:编译出来的PC端串口工具
| |->u-boot.bin: BSP29默认编译出来的u-boot.bin.
Product Category
NXP Part Number
URL
Auto MPU
S32G274
https://www.nxp.com/s32g
View full article