Vibration Monitoring - Prediction using NXP Sensors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vibration Monitoring - Prediction using NXP Sensors

Vibration Monitoring - Prediction using NXP Sensors

Demo Owner michaelestanley

By monitoring the vibration signature of a rotating machinery we can predict the remaining useful life of that machine.

Features

  • Condition monitoring
  • Visual characterization of the fundamental frequency of a  motor along with its harmonics
  • Features that can be observed: wavelength, transfer coefficients, statistical measures, standard deviations, variances
  • Preparing work flows where users can use machine learning algorithms to to figure out what feature sets are important, focusing only on the features that are needed to predict the remaining useful life of the machine


Links

标签 (1)
无评分
版本历史
最后更新:
‎06-30-2014 03:27 PM
更新人:
NXP Employee