Vibration Monitoring - Prediction using NXP Sensors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vibration Monitoring - Prediction using NXP Sensors

Vibration Monitoring - Prediction using NXP Sensors

Demo Owner michaelestanley

By monitoring the vibration signature of a rotating machinery we can predict the remaining useful life of that machine.

Features

  • Condition monitoring
  • Visual characterization of the fundamental frequency of a  motor along with its harmonics
  • Features that can be observed: wavelength, transfer coefficients, statistical measures, standard deviations, variances
  • Preparing work flows where users can use machine learning algorithms to to figure out what feature sets are important, focusing only on the features that are needed to predict the remaining useful life of the machine


Links

ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎06-30-2014 03:27 PM
更新者:
NXP Employee