Machine Vision Demo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Machine Vision Demo

Machine Vision Demo

Demo Owner: David Chung

Intended to demonstrate how one can leverage NXP technology to safely transport loads in a range of settings from a shipyard to an assembly line.

Demo runs a Seavus developed application that pre-calculates a path based on environmental input given by the QorIQ LS1021A.  It then moves the load according to that path, adjusting for unforeseen hazards such as people who move in the way during transport.  It ensures that the landing area is clear before dropping the load.

Demo is entire self-contained.

 

 

Features

QorIQ LS1021A

  • FPU for precise mathematical computation
  • IEEE 1588 Precision Time Protocol to sync clocks within system
  • WiFi connectivity to Human-Machine Interface
  • SEC 5.5 crypto accelerator for maximum security
  • Dual core for redundancy

i.MX6

  • Specialized imaging processor
  • Used as camera interface to facilitate trajectory calculation

Kinetis Microcontroller K40

  • General purpose low power MCU
  • Utilized to control the crane's stepper motor

Green Hills INTEGRITY RTOS

  • Certified EAL6+ High Robustness by NSA
  • Separates critical and non-critical tasks

Seavus Crane Application

  • Efficient algorithm for trajectory calculation and load transport

Block Diagrams

Organizational Structure

17820_17820.pngBlockDiagram3.png

Algorithm Diagram

16494_16494.pngBlockDiagram2.png

Function Allocation

17821_17821.pngFunctionAllocation.png

 

标签 (1)
评论

Cool demo David.  I would really like to see this demo presented in the context of a DIY'er pick-and-place type of machine.  Seems like you have most of the hardware already for it.

Anonymous

Hi John,

Thank you for your interest.  The demo is currently being remodeled to include i.MX and Kinetis.  John Ralston is the expert to contact about the demo.  Hope this helps.

-David

无评分
版本历史
最后更新:
‎11-11-2014 01:32 PM
更新人:
Anonymous