read PN7150 binary file but response error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

read PN7150 binary file but response error

1,057件の閲覧回数
cuh
Contributor I

Hi all

I just study the NFC with STM32F429. The device host connect NFC with I2C and I can read the VID/PID.

But I can't read the binary file content.

Command1: 00 a4 04 00 07
Response1: 00 00 02 90 00
Command2: 00 a4 00 0c 02
Response2: 00 00 02 90 00
Command3: 00 b0 00 00 02 
Response3: 00 00 04 04 60 90 00
Command4: 00 b0 00 02 b0 
Response4: 60 06 03 01 00 01

Can Anyone help me what is the "60 06 03 01 00 01" and how to fix it?
Regards,



タグ(1)
0 件の賞賛
返信
0 返答(返信)