read PN7150 binary file but response error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

read PN7150 binary file but response error

1,074 Views
cuh
Contributor I

Hi all

I just study the NFC with STM32F429. The device host connect NFC with I2C and I can read the VID/PID.

But I can't read the binary file content.

Command1: 00 a4 04 00 07
Response1: 00 00 02 90 00
Command2: 00 a4 00 0c 02
Response2: 00 00 02 90 00
Command3: 00 b0 00 00 02 
Response3: 00 00 04 04 60 90 00
Command4: 00 b0 00 02 b0 
Response4: 60 06 03 01 00 01

Can Anyone help me what is the "60 06 03 01 00 01" and how to fix it?
Regards,



Tags (1)
0 Kudos
Reply
0 Replies