problems with PN5180 Python library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problems with PN5180 Python library

Jump to solution
5,897 Views
Konrad007
Contributor I

Hey,

I'm looking for a python library which I can use on a Raspberry Pi 4 with my PN5180 NFC reader (only with the pins on the Raspberry Pi). I've already tried a library  which I found on github(https://github.com/fservida/pyPN5180),  but if I held a NFC/RFID Tag (ISO/IEC 14443A)  near the reader it hasn't detected any tag. Now I can't find the problem and look for a good python library wich supports the ISO/IEC 14443A. Can someone recommend a library? 

regards Konrad

0 Kudos
Reply
1 Solution
5,806 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your update information. Yes. PN7150 supports Android.

For the more information please refer to the document.

URL:https://www.nxp.com/docs/en/application-note/AN11690.pdf.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

 

 

View solution in original post

0 Kudos
Reply
4 Replies
5,833 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately. We have not the library for the application.

 But PN7150 which has a library supporting NCI interface, but we don't have python example.
Please refer to https://github.com/NXPNFCLinux/linux_libnfc-nci and 
https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Easy-set-up-of-NFC-on-Raspberry-Pi/ta-p/1099....

 Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply
5,829 Views
BANGYUD
Contributor II

hi sir , how about PN7150 with android ,did pn7150 support for android , if did,  did you have document for intergrating both of it , 
thanks a lot 

0 Kudos
Reply
5,806 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your update information. Yes. PN7150 supports Android.

For the more information please refer to the document.

URL:https://www.nxp.com/docs/en/application-note/AN11690.pdf.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

 

 

0 Kudos
Reply
5,846 Views
BANGYUD
Contributor II

have you found that ?

0 Kudos
Reply