pn5180-icode xli x2 read password err

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pn5180-icode xli x2 read password err

2,411 Views
guangshi
Contributor I

first get random

guangshi_1-1607675859238.png

detal:

send 09 00 22 b2 04 + UID

rev 00 xx xx(randdom number)

xx Rand[0] Rand[2]

xx Rand[1] Rand[3]

then XOR_password

guangshi_2-1607675941143.png

detal:password 0000 0000(original password)

In the end! Set read password

send 09 00 22 b3 04 +UID +01(read type) +XOR_password

rev 01 0f 

Final reply error.

Are my steps correct?

Tags (1)
0 Kudos
Reply
4 Replies

2,376 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi @guangshi ,

Hope you are doing great the process for this should be :

  1. activate the ICODE by sending the inventory command
  2. select the ICODE you want with the select command
  3. get random number 
  4. set password, for the PWD ID you want to use:
    • 01- Read
    • 02 - Write
    • 04 - privacy
    • 08 - Destroy
    • 10 EAS/AFI

you can find a script I just did for you doing the above process for the ICODE SLIX2 and Read PWD.

Hope this information helps.

Have a great day!

 

BR

 

Jonathan

0 Kudos
Reply

2,384 Views
AlanSbor
Contributor II

/*
* The SET PASSWORD command enables the different passwords to be transmitted to the label
* to access the different protected functionalities of the following commands.
* The SET PASSWORD command has to be executed just once for the related passwords if the label is powered
*/
ISO15693ErrorCode PN5180ISO15693::setPassword(uint8_t *password, uint8_t *random) {
uint8_t setPassword[] = {0x02, 0xB3, 0x04, 0x04, 0x00, 0x00, 0x00, 0x00};
uint8_t *readBuffer;
setPassword[4] = password[0] ^ random[0];
setPassword[5] = password[1] ^ random[1];
setPassword[6] = password[2] ^ random[0];
setPassword[7] = password[3] ^ random[1];
ISO15693ErrorCode rc = issueISO15693Command(setPassword, sizeof(setPassword), &readBuffer);
return rc;
}

ISO15693ErrorCode PN5180ISO15693::enablePrivacy(uint8_t *password, uint8_t *random) {
uint8_t setPrivacy[] = {0x02, 0xBA, 0x04, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t *readBuffer;
setPrivacy[3] = password[0] ^ random[0];
setPrivacy[4] = password[1] ^ random[1];
setPrivacy[5] = password[2] ^ random[0];
setPrivacy[6] = password[3] ^ random[1];
ISO15693ErrorCode rc = issueISO15693Command(setPrivacy, sizeof(setPrivacy), &readBuffer);
return rc;
}

0 Kudos
Reply

2,385 Views
AlanSbor
Contributor II

// ICODE SLIX specific commands

/*
* The GET RANDOM NUMBER command is required to receive a random number from the label IC.
* The passwords that will be transmitted with the SET PASSWORD,ENABLEPRIVACY and DESTROY commands
* have to be calculated with the password and therandom number (see Section 9.5.3.2 "SET PASSWORD")
*/
ISO15693ErrorCode PN5180ISO15693::getRandomNumber(uint8_t *randomData) {
uint8_t getrandom[] = {0x02, 0xB2, 0x04};
uint8_t *readBuffer;
ISO15693ErrorCode rc = issueISO15693Command(getrandom, sizeof(getrandom), &readBuffer);
if (rc == ISO15693_EC_OK) {
randomData[0] = readBuffer[1];
randomData[1] = readBuffer[2];
}
return rc;
}

0 Kudos
Reply

2,410 Views
guangshi
Contributor I

guangshi_0-1607676706955.png

 

0 Kudos
Reply