mfrc630 communicating android with nfc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfrc630 communicating android with nfc

2,746件の閲覧回数
gksrb4
Contributor I

hi, Is mfrc630 supported to communicate android smartphone? if so, which iso is used?

ラベル(2)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,588件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

In theory a reader can communicate with another reader in the following scenarios:

1. Peer to peer.

2. Card emulation.

It will be necessary to define in which NFC mode they will be working and set to each side.

Best regards,

Ivan.

0 件の賞賛
返信

2,588件の閲覧回数
gksrb4
Contributor I

in doc, MFRC630 and MFRC630 plus: High-performance frontend for MIFARE and NTAG products Rev. 4.7 — 12 September 2018

The MFRC630 multi-protocol NFC frontend IC supports the following operating modes:

• Read/write mode supporting ISO/IEC 14443A and MIFARE Classic -> this is mifare i know

• Read/write mode supporting NTAG 

what is NTAG? Is it reader can imitate card role?

1. Peer to peer.-> Is this supported by mfrc630?

2. Card emulation. -> Are you talking about smartphone card emulation mode?

0 件の賞賛
返信

2,588件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

NTAG is a Tags family, for more information, please refer to: https://www.nxp.com/products/identification-security/rfid/nfc-hf/ntag:MC_71717

Regarding the NFC Frontends, please take a look to the NFC Frontend solutions in the following link for the NFC Functionality: https://www.nxp.com/docs/en/brochure/939775017564.pdf

Hope this helps.

Best regards,

Ivan.

0 件の賞賛
返信