hello ,I check clrc663's datasheet in 8.8.2 part( The CLRC663 is able to provide a clock with configurable frequency at CLKOUT from 1 MHz to 24 MHz
(PLL_Ctrl and PLL_DIV). There it can serve as a clock source to a microcontroller which avoids the need of
a second crystal oscillator in the reader system. Clock source for the IntegerN-PLL is the 27.12 MHz crystal
oscillator ).
I want to use clkout of Clrc663 for MCU's clkin in reader system,how to change clrc663's eeprom to achieve the function?