What is the maximum length of commands/responses using the DNA ICode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the maximum length of commands/responses using the DNA ICode?

828件の閲覧回数
chuckdosh
Contributor I

With the DNA RFID (SL2S6002 ICODE), what is the byte length of the longest RF command

What is the longest RFID response possible for this tag?

Example:

To read all 64 blocks with write protect flag, a long response may take 1 (status) + 64*(4+1) + 2 (crc) or 323 bytes.

icodeDNA‌

タグ(1)
0 件の賞賛
返信
0 返答(返信)