Using CLRC663 to test ILT tag effective?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using CLRC663 to test ILT tag effective?

1,686件の閲覧回数
m4416202
Contributor I

Hello

      I already used the CLRC663 blue board to test ILT tags.But I have some questions about it.

1、How to change the CLRC663 blue board and make it use 50oh  SMA cable?(it has RXN and RXP receive ports)

2、The blue board works on 13.56MHz,But the frequency point of ILT tags locates at 80MHz~100MHz。Did i need to change somethings when i use blue board to test ILT tags?

0 件の賞賛
返信
1 返信

1,524件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

>>1、How to change the CLRC663 blue board and make it use 50oh  SMA cable?(it has RXN and RXP receive ports)

Not recommoned you change antenna of CLRC663 bule board, easy to damage RC663 board! If you want to design your own products based on CLRC663, You can use single-end antenna with 50OHM, for this, we can provide a reference, you can submit a case to get it via our salesforce system.

>>2、The blue board works on 13.56MHz,But the frequency point of ILT tags locates at 80MHz~100MHz。Did i need to change somethings when i use blue board to test ILT tags?

>>ILT tag's frequency seems alos 13.56MHz, see our product ICODE ILT:

http://www.nxp.com/documents/data_sheet/SL2S1402_SL2S1502_SL2S1602.pdf 

Best Regards,

weidong

0 件の賞賛
返信