Using CLRC663 to test ILT tag effective?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using CLRC663 to test ILT tag effective?

1,683 Views
m4416202
Contributor I

Hello

      I already used the CLRC663 blue board to test ILT tags.But I have some questions about it.

1、How to change the CLRC663 blue board and make it use 50oh  SMA cable?(it has RXN and RXP receive ports)

2、The blue board works on 13.56MHz,But the frequency point of ILT tags locates at 80MHz~100MHz。Did i need to change somethings when i use blue board to test ILT tags?

0 Kudos
Reply
1 Reply

1,521 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

>>1、How to change the CLRC663 blue board and make it use 50oh  SMA cable?(it has RXN and RXP receive ports)

Not recommoned you change antenna of CLRC663 bule board, easy to damage RC663 board! If you want to design your own products based on CLRC663, You can use single-end antenna with 50OHM, for this, we can provide a reference, you can submit a case to get it via our salesforce system.

>>2、The blue board works on 13.56MHz,But the frequency point of ILT tags locates at 80MHz~100MHz。Did i need to change somethings when i use blue board to test ILT tags?

>>ILT tag's frequency seems alos 13.56MHz, see our product ICODE ILT:

http://www.nxp.com/documents/data_sheet/SL2S1402_SL2S1502_SL2S1602.pdf 

Best Regards,

weidong

0 Kudos
Reply