TDA8024TT VDD question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TDA8024TT VDD question

ソリューションへジャンプ
2,681件の閲覧回数
jackylu
Contributor II

Hi,

Would you please help to check as below?

(1) any restriction for the power sequence of VDD(supply voltage 3.3V) and VDDP(DC-DC supply voltage 5V) (2) Will TDA8024TT be broken when VDD is 0V & VDDP is 5V?

ラベル(1)
タグ(1)
1 解決策
2,459件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi, jacky

(1) any restriction for the power sequence of VDD(supply voltage 3.3V) and VDDP(DC-DC supply voltage 5V)

No, there is no restriction. TDA8024 and the microcontroller must use the same VDD supply.

See applicaton diagram in TDA8024 datasheet, please! page 24.

(2) Will TDA8024TT be broken when VDD is 0V & VDDP is 5V?

If VDD is 0v, TDA8024TT can't communicate with microcontorller.
because VDD is for Host I/O, even TDA8024TT's reset pin will be low level,
it means TDA8024TT couldn't work.

Have a nice day!

TIC weidong sun

元の投稿で解決策を見る

2 返答(返信)
2,460件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi, jacky

(1) any restriction for the power sequence of VDD(supply voltage 3.3V) and VDDP(DC-DC supply voltage 5V)

No, there is no restriction. TDA8024 and the microcontroller must use the same VDD supply.

See applicaton diagram in TDA8024 datasheet, please! page 24.

(2) Will TDA8024TT be broken when VDD is 0V & VDDP is 5V?

If VDD is 0v, TDA8024TT can't communicate with microcontorller.
because VDD is for Host I/O, even TDA8024TT's reset pin will be low level,
it means TDA8024TT couldn't work.

Have a nice day!

TIC weidong sun

2,459件の閲覧回数
jackylu
Contributor II

Dear Sir,

Good day,

My customer wants to know TDA8024TT/C1 Tj operating maximum temperature.

Do yo have this information?

Thanks

 

0 件の賞賛
返信