SetConfiguration Command length error ntag 424

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SetConfiguration Command length error ntag 424

997件の閲覧回数
zahra2023
Contributor III

Hi,

I want to run setConfiguration command and according to NT4H2421Gx PDF the command should be like : [ 0x90,0x5C,0x00,0x00,0x06,0x0A,0x00,0x00,0x00,0x00,0x00,0x00]

Lc 0x06 : Data Parameters length is 5 + 1 (option = 0x0A)

Option : 0x0A => Failed authentication counter setting

Data (FailedCtrOption) : 0x00 => it 0: Set to 0b for disabling

but it return 7Eh (Option 0Ah: Data length is not 5) while is 5 !

Any help appreciated.
タグ(2)
0 件の賞賛
返信
0 返答(返信)