SetConfiguration Command length error ntag 424

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SetConfiguration Command length error ntag 424

1,007 Views
zahra2023
Contributor III

Hi,

I want to run setConfiguration command and according to NT4H2421Gx PDF the command should be like : [ 0x90,0x5C,0x00,0x00,0x06,0x0A,0x00,0x00,0x00,0x00,0x00,0x00]

Lc 0x06 : Data Parameters length is 5 + 1 (option = 0x0A)

Option : 0x0A => Failed authentication counter setting

Data (FailedCtrOption) : 0x00 => it 0: Set to 0b for disabling

but it return 7Eh (Option 0Ah: Data length is not 5) while is 5 !

Any help appreciated.
0 Kudos
Reply
0 Replies