Problems connecting to CLEV6640B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems connecting to CLEV6640B

1,872 Views
fredrik_jagenhe
Contributor I

Hi,

I have problems connecting to my CLEV6640B board. It used to work, but no longer. Not sure what has happened with it since, it asked me about firmware updates when connecting it to NXP NFC Cockpit which I gave it and now it no longer wants to talk with the application.

The following is printed in the application when I connect to the port:

[2019.03.18 16:12:15]:INFO:ServiceFactory:Generating Services for VCOM_RC663 @\\.\COM13
[2019.03.18 16:12:16]:ERROR:ServiceFactory:halRc663.ApplyProtocolSettings() Failed. Status=HAL,BUFFER_OVERFLOW
[2019.03.18 16:12:16]:ERROR:ServiceFactory:m_bal.SetConfig(HalHwType,RC663) failed. Status=HAL,BUFFER_OVERFLOW
[2019.03.18 16:12:16]:ERROR:ServiceFactory:generateServices(VCOM_RC663 @\\.\COM13) Failed with HAL,BUFFER_OVERFLOW
[2019.03.18 16:12:16]:INFO:ServiceFactory:uC FW Version: NNC_uC_VCOM_03.04.00_20180420 (Compiled on Apr 20 2018 19:05:55)
[2019.03.18 16:12:16]:ERROR:ServiceFactory:SelectBalHalOsal(selected_board) Failed with HAL,BUFFER_OVERFLOW

When connecting a scope on the SPI lines between the LPC and the CLRC663, it seems that he CLRC663 is communicating with the LPC. I did not decode the communication however to make sure the commands made sense.

I reflashed the LPC code using the firmware BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin from NXP NFC Cockpit v4.8.0 but it did not help.

I verified that NXP NFC Cockpit v4.8.0 could communicate with a card (thus ruling out issues with the USB drivers) using another CLEV6640B board and it worked without any problems.

This leaves the CLRC663 as a possible failure source. Is there any way I can reprogram the CLRC663 if this is the case?

Tags (1)
0 Kudos
Reply
1 Reply

1,680 Views
Kan_Li
NXP TechSupport
NXP TechSupport

There is a firmware update guide for PNEV5180, but can also apply for CLEV6630B, please kindly refer to Program the firmware to PNEV5180B board for details.

Hope that helps,


Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply