Please Help me! How I can set registers below to active interrupt (IRQ) without send command via SPI? After configured registers active IRQ when card is near, without send command. Is possible? Thank you. WriteRawRC(DivlEnReg, 0x84); // WriteRawRC(Div

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Please Help me! How I can set registers below to active interrupt (IRQ) without send command via SPI? After configured registers active IRQ when card is near, without send command. Is possible? Thank you. WriteRawRC(DivlEnReg, 0x84); // WriteRawRC(Div

2,650件の閲覧回数
marcosriolo
Contributor I

Please Help me! How I can set registers below to active interrupt (IRQ) without send command via SPI?

After configured registers active IRQ when card is near, without send command.

Is possible?

Thank you.

WriteRawRC(DivlEnReg, 0x84); //
WriteRawRC(DivIrqReg, 0x80); //
WriteRawRC(ComIEnReg, 0xA0); //
WriteRawRC(ComIrqReg, 0x80);
ClearBitMask(ComIrqReg, 0x80); //
WriteRawRC(FIFODataReg, PICC_REQIDL);
WriteRawRC(CommandReg,PCD_TRANSCEIVE);
WriteRawRC(BitFramingReg, 0x87);

0 件の賞賛
返信
5 返答(返信)

2,400件の閲覧回数
marcosriolo
Contributor I

Please, give me example to set registrers: (Send IRQ without command SPI)

CommandReg

ComIEnReg

DivIEnReg

0 件の賞賛
返信

2,400件の閲覧回数
jconvex
Contributor I

Are you success to send IRQ without command SPI when a new card come in the RF field?

0 件の賞賛
返信

2,401件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Marcos Riolo,

Actually the command is written into the CommandReg register, while interrupts enablement is controled by ComIEnReg and DivIEnReg registers, so it is possible to active IRQ without sending command via SPI.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,401件の閲覧回数
marcosriolo
Contributor I

Dear, the device is IC  RC522. working via SPI.

0 件の賞賛
返信

2,401件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Marcos Riolo,

I am sorry , but which device are you working on? Would you please help to specify it? Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信