if the tag support power harvesting function, the PN553 can work it well? can supply the engery(~10mA) to such tag circuit
Hello,
It depends on many parameters, such as the antenna design and the antenna proximity to the tag. The closer, the more power provided to the tag.
Are you working with NTAG I2C Plus?
Regards,
Ivan.
Hi Ivan, Could you please help give the reply on my question, tks a lot!
Could you please help check my question? Tks a lot in advance!
Hi Ivan,
share you the NFC COIL spec:
La | Rs | Rp | Fra | Q | |
NFC 13.56MHz | 1~2uH | <1.2Ohm | >1K | >30M | >15 |
the distannce between COIL and tag should be about 2.36mm
the customer use the NFC tag chip as this link: Silicon Craft Technology :: SIC4310
could you please help check that can work well(supply 10mA for the tag circuit)
BRS,
TONY LIU