Please Help me! How I can set registers below to active interrupt (IRQ) without send command via SPI? After configured registers active IRQ when card is near, without send command. Is possible? Thank you. WriteRawRC(DivlEnReg, 0x84); // WriteRawRC(Div

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please Help me! How I can set registers below to active interrupt (IRQ) without send command via SPI? After configured registers active IRQ when card is near, without send command. Is possible? Thank you. WriteRawRC(DivlEnReg, 0x84); // WriteRawRC(Div

2,652 Views
marcosriolo
Contributor I

Please Help me! How I can set registers below to active interrupt (IRQ) without send command via SPI?

After configured registers active IRQ when card is near, without send command.

Is possible?

Thank you.

WriteRawRC(DivlEnReg, 0x84); //
WriteRawRC(DivIrqReg, 0x80); //
WriteRawRC(ComIEnReg, 0xA0); //
WriteRawRC(ComIrqReg, 0x80);
ClearBitMask(ComIrqReg, 0x80); //
WriteRawRC(FIFODataReg, PICC_REQIDL);
WriteRawRC(CommandReg,PCD_TRANSCEIVE);
WriteRawRC(BitFramingReg, 0x87);

0 Kudos
Reply
5 Replies

2,402 Views
marcosriolo
Contributor I

Please, give me example to set registrers: (Send IRQ without command SPI)

CommandReg

ComIEnReg

DivIEnReg

0 Kudos
Reply

2,402 Views
jconvex
Contributor I

Are you success to send IRQ without command SPI when a new card come in the RF field?

0 Kudos
Reply

2,403 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Marcos Riolo,

Actually the command is written into the CommandReg register, while interrupts enablement is controled by ComIEnReg and DivIEnReg registers, so it is possible to active IRQ without sending command via SPI.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,403 Views
marcosriolo
Contributor I

Dear, the device is IC  RC522. working via SPI.

0 Kudos
Reply

2,403 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Marcos Riolo,

I am sorry , but which device are you working on? Would you please help to specify it? Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply