PN7XXX Family flash programing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7XXX Family flash programing

2,491件の閲覧回数
damianogilioli
Contributor I

Hi All,

I'm using a PN7362 and I'd like to perform a flash programming via SWD (with LPCXpresso) without the IDE MCUXpresso but with a simple Software like Flash Magic. Unfortunately I'm not able to perform the programming with Flash Magic because doesn't support PN7XXX family. Is available unother PC software?

Thank you

0 件の賞賛
返信
3 返答(返信)

2,194件の閲覧回数
damianogilioli
Contributor I

Hello, 

thank you Kan Li for the reply.

I'd like to perform the programming with LPC-Link 2, Is there another PC Software avalilable?

0 件の賞賛
返信

2,194件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello,

LPC-Link 2 can be used as a jlink, please refer to LPCScrypt v2.1.0 | NXP for details.

Hope that helps,


Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,194件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello,

You may try jlink instead. Please refer to the following for details.

pastedImage_1.png


Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信