PN7642 code read protect

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7642 code read protect

Jump to solution
2,710 Views
artem_pn
Contributor II

Hello! 

I am using PN7642 in my project. I would like to ask, how to protect code from reading properly?

In the datasheet I found description of CRP Levels (CRP1, CRP2, CRP3).  In library the is function PN76_Status_t PN76_Sys_OTPConfigs_EnableCRP(). I would like to ask how to use it properly? Where in code it should be called? What level of code read protection it provides? How to check if it works? 

I called it from main() function, it returned 0x07 value (what can cause that? it seems like possible values are 0x00 and 0x08) and I still can read memory using JLink utility. 

Thank you in advance!

Artem 

0 Kudos
Reply
1 Solution
2,669 Views
jimmychan
NXP TechSupport
NXP TechSupport

Please open the API User documentation.

2025-03-26 12_49_34-AN13936.pdf - Adobe Acrobat Reader (32-bit).png

 

Then go to the OTP (One Time Programable) calls:

2025-03-26 12_48_05-PN7642 NFC Controller_ SYS OTP Config Interface.png

 

You could find all kind of security features to protect the chip such as Read protection, SWD disable and so on.

 

View solution in original post

0 Kudos
Reply
3 Replies
2,670 Views
jimmychan
NXP TechSupport
NXP TechSupport

Please open the API User documentation.

2025-03-26 12_49_34-AN13936.pdf - Adobe Acrobat Reader (32-bit).png

 

Then go to the OTP (One Time Programable) calls:

2025-03-26 12_48_05-PN7642 NFC Controller_ SYS OTP Config Interface.png

 

You could find all kind of security features to protect the chip such as Read protection, SWD disable and so on.

 

0 Kudos
Reply
2,466 Views
KB1
Contributor II

I also am getting a 0x07 return code.  The API documentation you pointed to has no useful information about what code 7 "PN76_STATUS_AUTH_ERROR" means or how to deal with it.

Can you please provide more information on how to utilize the Code Read Protection functionality in the chip?

 

0 Kudos
Reply
2,410 Views
artem_pn
Contributor II

Hello!

The function PN76_Sys_OTPConfigs_EnableCRP() can be called only once. After that trying to debug it, I have got this 0x07 message, but it turned off an ability for me to run device in USB FW update mode by selecting boot from USB on evaluation board

0 Kudos
Reply