PN7462 remap(vector table)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7462 remap(vector table)

3,276 次查看
youngseo
Contributor I

Hello,

I want to use the PN7462 to create a bootloader (0x203000) and an application (0x204000).

Once I created a bootloader and jumped to the application (0x204000) area.

However, when application (0x204000) is executed, it stops.

I need to modify the vector table, but I do not know how to do it.

In the case of LPC series, it seems to move using SYSMEMREMAP or VTOR, but PN7462 does not seem to exist.

I am wondering how the PN7462 modifies the Vector Table.

0 项奖励
回复
3 回复数

3,032 次查看
adriancano
NXP Employee
NXP Employee

Hi,

Cortex M0 does not allow vector table to be remapped. Therefore, secondary bootloader has to be designed to redirect the processor to the handler listed in a vector table located in the applicat are of flash memory.

Please refer to AN10995 document and software that presents a Secondary Bootloader application for LPC1100.

https://www.nxp.com/docs/en/application-note/AN10995.zip 

Hope the information helps.

0 项奖励
回复

3,032 次查看
youngseo
Contributor I

Thank you for answer.

But, I am difficult to understand the sentence below.

" Therefore, secondary bootloader has to be desined to redirect the processor to the handler listed in a vector table located in the applicat are of flash memory."

Please give more specific explanation.

Best Regards.

0 项奖励
回复

3,032 次查看
adriancano
NXP Employee
NXP Employee

Hi, The information is part of the document I pointed, AN10995, please go through the document and you will find a better explanation of my sentence.

Regards

0 项奖励
回复