PN7462 RX optimization for ISO14443A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 RX optimization for ISO14443A

1,587件の閲覧回数
bds1
Contributor I

I'm trying to optimize the PN7462 RX parameters (RxHpcf, RxGain and MinLevel) for ISO14443A card detection and communication. I have a few questions about this:

- Is there a documented procedure to do this?

- Which RxHpcf, RxGain and MinLevel EEPROM parameters are used during technology detection, collision resolution and activation?

- Which RxHpcf, RxGain and MinLevel EEPROM parameters are used during ISO14443A communication at 106 kbps?

0 件の賞賛
返信
1 返信

1,487件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

You can read the values stored in EEPROM by making use of the cockpit tool. So that you can take them as reference: 

NFC Cockpit|NXP 

I hope this helps.

Reagards,

Ivan.

0 件の賞賛
返信