PN7462 How to Disable RfPower Dynamic Power Control From Firmware?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 How to Disable RfPower Dynamic Power Control From Firmware?

Jump to solution
1,662 Views
EE_Ark
Contributor II

Hi,

I'm using PN7462 in my project.

I want to disable RfPower "Dynamic Power Control" feature.

It looks like this feature is controlled by bit0(DPC_ENABLE) of 'bOcProtControl' byte in phCfg_EE_HW_RfDPC.

 

But I don't want to generate a new eeprom file and burn this eeprom into my devices.

What I want to do is no matter what is written in the relevant section of the eeprom file, this feature should be turned off at the beginning of my firmware.

How can I do this?

 

0 Kudos
Reply
1 Solution
1,630 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @EE_Ark 

 

I would suggest you refer to AN 11742,  there is a DPC_CONTROL register responsible for enable/disable DPC function.

danielchen_0-1699236190031.png

 

 

Regards

Daniel

 

View solution in original post

0 Kudos
Reply
1 Reply
1,631 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @EE_Ark 

 

I would suggest you refer to AN 11742,  there is a DPC_CONTROL register responsible for enable/disable DPC function.

danielchen_0-1699236190031.png

 

 

Regards

Daniel

 

0 Kudos
Reply