PN7462 How to Disable RfPower Dynamic Power Control From Firmware?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 How to Disable RfPower Dynamic Power Control From Firmware?

ソリューションへジャンプ
1,666件の閲覧回数
EE_Ark
Contributor II

Hi,

I'm using PN7462 in my project.

I want to disable RfPower "Dynamic Power Control" feature.

It looks like this feature is controlled by bit0(DPC_ENABLE) of 'bOcProtControl' byte in phCfg_EE_HW_RfDPC.

 

But I don't want to generate a new eeprom file and burn this eeprom into my devices.

What I want to do is no matter what is written in the relevant section of the eeprom file, this feature should be turned off at the beginning of my firmware.

How can I do this?

 

0 件の賞賛
返信
1 解決策
1,634件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @EE_Ark 

 

I would suggest you refer to AN 11742,  there is a DPC_CONTROL register responsible for enable/disable DPC function.

danielchen_0-1699236190031.png

 

 

Regards

Daniel

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,634件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @EE_Ark 

 

I would suggest you refer to AN 11742,  there is a DPC_CONTROL register responsible for enable/disable DPC function.

danielchen_0-1699236190031.png

 

 

Regards

Daniel

 

0 件の賞賛
返信