PN7160 matching with DPC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7160 matching with DPC

1,397件の閲覧回数
michael_d_1983
Contributor I

Hello,

According to the antenna matching guide, asymmetric matching is used for the OM27160 demo board (fr0 = 22MHz).

According to the circuit diagram for the demo board, the filter frequency is 14.5MHz (160nH, 750pF), so symmetrical is used which, according to the antenna matching guide, requires DPC ?

In the source code (I use the MCUXpresso library) nothing indicates that DPC is used.

Does the demo project use DPC and what filter value is recommended?

I designed and calculated my own board with a slightly larger antenna and achieve extremely poor results with a fr0 with 22MHz and only passable with 14.5MHz.

The antenna data was determined with a network analyzer, the matching circuit with the online tool and the PN7160 matching calculator.

Where can I start to get better results? (Increase Q, increase fr0, ...)

How can I restore the default values ​​of the NxpNci_RF_CONF? The default values ​​are not mentioned in the UM.

Thanks very much,
Michael

0 件の賞賛
返信
1 返信

1,336件の閲覧回数
michael_d_1983
Contributor I

How can I restore the default values ​​of the NxpNci_RF_CONF? The default values ​​are not mentioned in the UM.

Thanks very much,
Michael

0 件の賞賛
返信