PN7160/PN7161 DPC Symmetric Tuning Values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7160/PN7161 DPC Symmetric Tuning Values

Jump to solution
1,437 Views
joshgott
Contributor I

For the PN7160 and PN7161, NXP recommends the following: "To use symmetrical tuning function + Dynamic Power Control (DPC), target the target impedance 16R for V_TVDD = 5V, and 11R for V_TVDD=3.3V respectively." Does NXP have target impedance values for V_TVDD values between 3.3V and 5V? For example, if I wanted V_TVDD=4V, what should I set my target impedance to be? A look up table or something similar would be much appreciated.

0 Kudos
Reply
1 Solution
1,419 Views
Tomas_Parizek
NXP Employee
NXP Employee

Hello joshgott, 

See the excel calculator in the attachment. Based on the inputs values (VDD voltage and complex impedance), you can calculate the expected TVDD current. 

See an example below.

For V_TVDD=4V, and target impedance (14-1i) Ohm. The target current would be approx. 220 mA

Tomas_Parizek_0-1722494318266.png

Please note that this calculation is a bit simplified. So if possible, we recommend to measure the current after the impedance tuning. 

BR

Tomas 

 

 

 

View solution in original post

1 Reply
1,420 Views
Tomas_Parizek
NXP Employee
NXP Employee

Hello joshgott, 

See the excel calculator in the attachment. Based on the inputs values (VDD voltage and complex impedance), you can calculate the expected TVDD current. 

See an example below.

For V_TVDD=4V, and target impedance (14-1i) Ohm. The target current would be approx. 220 mA

Tomas_Parizek_0-1722494318266.png

Please note that this calculation is a bit simplified. So if possible, we recommend to measure the current after the impedance tuning. 

BR

Tomas