PN7160 DPC check

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
72,095件の閲覧回数
Alb
Contributor I

Hi,

I'm trying to setup dpc on pn7160 (AN13224) but when I select "12"->DPC Check on "NfcFactoryTestApp" I get the answer "Error, cannot get parameter value". Buffer received is 4F 3F 01 09. Can you tell me which is the reason of failure and most important where I can find this info in nxp docs?

Thanks

Alberto

 

0 件の賞賛
返信
1 解決策
71,552件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello mark_tang, 

I see your PN7160 FW version is 12.50.05

Tomas_Parizek_0-1688464972452.png

As Alberto has mentioned, the DPC Check has been added from version 12.50.06.

Tomas_Parizek_1-1688465061525.png

I am sorry that I overlooked this fact. I assumed that the FW you have is 06 or higher. 

So the DPC is working but the DPC command is not supported for the 05 FW version. 

The FW update can be done as described here: 

The latest FW, you can find it here -> https://github.com/NXP/nfc-NXPNFCC_FW/tree/master/InfraFW/pn7160

More description of how to do the FW update is available in PN7160 FAQ document -> 19 FW update

https://www.nxp.com/docs/en/application-note/AN13892.pdf 

BR

Tomas 

 

 

元の投稿で解決策を見る

28 返答(返信)
24,719件の閲覧回数
Alb
Contributor I

Hi Daniel,

I will check parameters but can you tell me the meaning of device answer I reported for "DPC check" command in the app? I would like to have a clarification about it becasue using this setup reader works perfectly....

Thanks

Alberto

 

0 件の賞賛
返信
24,063件の閲覧回数
mark_tang
Contributor I

Hi Alberto:

I'm having the same issue, have you already solved it  (Android 13 ),the current is 032E  without card in  the proximity.When Placing an card  in the proximity ,the current is 037F

DPC-HELPER-fail.PNGDPC-HELPER-RSP.PNG

 

 

 

0 件の賞賛
返信
6,858件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello mark_tang

Could you share your "NfcFactoryTestApp.c" code, please? 

BR

Tomas 

0 件の賞賛
返信
6,773件の閲覧回数
mark_tang
Contributor I

Hi Tomas:

 This is for Android 13 and using I²C

 

0 件の賞賛
返信
71,553件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello mark_tang, 

I see your PN7160 FW version is 12.50.05

Tomas_Parizek_0-1688464972452.png

As Alberto has mentioned, the DPC Check has been added from version 12.50.06.

Tomas_Parizek_1-1688465061525.png

I am sorry that I overlooked this fact. I assumed that the FW you have is 06 or higher. 

So the DPC is working but the DPC command is not supported for the 05 FW version. 

The FW update can be done as described here: 

The latest FW, you can find it here -> https://github.com/NXP/nfc-NXPNFCC_FW/tree/master/InfraFW/pn7160

More description of how to do the FW update is available in PN7160 FAQ document -> 19 FW update

https://www.nxp.com/docs/en/application-note/AN13892.pdf 

BR

Tomas 

 

 

6,753件の閲覧回数
mark_tang
Contributor I
can you provide a link to download the newest?
0 件の賞賛
返信
6,737件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello mark_tang, 

You can find it here -> https://github.com/NXP/nfc-NXPNFCC_FW/tree/master/InfraFW/pn7160

More description of how to do the FW update is available in PN7160 FAQ document -> 19 FW update

https://www.nxp.com/docs/en/application-note/AN13892.pdf

 

BR

Tomas 

0 件の賞賛
返信
7,007件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello mark_tang, 

Thanks for your input! 

We are checking the topic internally in our labs. We will come back to you as soon as possible.

Thanks ! 

BR

Tomas 

 

0 件の賞賛
返信