PN7150 porting issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 porting issue

4,777件の閲覧回数
nanbaolin
Contributor I

Now we are debugging PN7150 on android Pie,but it seems the i2c error, Anybody know how to solve it ?

06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_sys_main.cc(133)] id=1, enable_cplt_mask=0x0
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_p2p_main.cc(477)] nfa_p2p_init
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_sys_main.cc(133)] id=3, enable_cplt_mask=0x8
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_rw_main.cc(70)] nfa_rw_init
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_sys_main.cc(133)] id=5, enable_cplt_mask=0x28
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_ce_main.cc(76)] nfa_ce_init
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_sys_main.cc(133)] id=6, enable_cplt_mask=0x68
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_ee_main.cc(97)] nfa_ee_init
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_sys_main.cc(133)] id=2, enable_cplt_mask=0x6c
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_hci_main.cc(192)] nfa_hci_init
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_sys_main.cc(133)] id=7, enable_cplt_mask=0xec
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:llcp_main.cc(57)] llcp_init
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:llcp_main.cc(89)] num_rx_buff = 9, rx_congest_start = 6, rx_congest_end = 4, max_num_ll_rx_buff = 2
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:llcp_main.cc(102)] max_num_tx_buff = 21, max_num_ll_tx_buff = 6
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:llcp_api.cc(369)] SAP:0x1, link_type:0x2, ServiceName:<urn:nfc:sn:sdp>
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:llcp_api.cc(453)] Registered SAP = 0x01
06-12 09:09:52.013 17963 17979 I libnfc_nci: [INFO:nfa_dm_api.cc(102)] NFA_Enable
06-12 09:09:52.015 17963 17983 I libnfc_nci: [INFO:nfa_sys_main.cc(77)] NFA got event 0x0100
06-12 09:09:52.015 17963 17983 I libnfc_nci: [INFO:nfa_dm_main.cc(121)] event: NFA_DM_API_ENABLE_EVT (0x00)
06-12 09:09:52.015 17963 17983 I libnfc_nci: [INFO:nfa_dm_act.cc(433)] nfa_dm_enable
06-12 09:09:52.015 17963 17981 I libnfc_nci: [INFO:gki_ulinux.cc(89)] gki_task_entry task_id=4, thread_id=787d5064f0/787d5064f0, pCond/pMutex=0x0/0x0
06-12 09:09:52.015 17963 17981 I libnfc_nci: [INFO:NfcAdaptation.cc(393)] NfcAdaptation::NFCA_TASK: enter
06-12 09:09:52.015 17963 17981 I libnfc_nci: [INFO:gki_ulinux.cc(450)] GKI_run enter
06-12 09:09:52.015 17963 17981 I libnfc_nci: [INFO:gki_ulinux.cc(460)] Start/Stop GKI_timer_update_registered!
06-12 09:09:52.016 17963 17981 I libnfc_nci: [INFO:gki_ulinux.cc(479)] GKI_run, run_cond(0x787dc466d8)=1
06-12 09:09:52.017 17963 17983 I libnfc_nci: [INFO:nfc_main.cc(664)] NFC_Enable
06-12 09:09:52.018 17963 17983 I libnfc_nci: [INFO:nfc_main.cc(326)] nfc_set_state 0 (NONE)->1 (W4_HAL_OPEN)
06-12 09:09:52.018 17963 17983 I libnfc_nci: [INFO:NfcAdaptation.cc(513)] NfcAdaptation::HalOpen
06-12 09:09:52.018   285   285 D [email protected]: Nfc::open_1_1(): enter
06-12 09:09:52.018   285   285 D [email protected]: Nfc::open(): enter
06-12 09:09:52.019   285   285 D NxpHal  : phNxpNci_MinOpen(): enter
06-12 09:09:52.019   285   285 E         : readConfig Cannot open config file /etc/libnfc-brcm.conf
06-12 09:09:52.019   285   285 D         : readNxpTransitConfig-Enter..Reading /data/vendor/nfc/libnfc-nxpTransit.conf
06-12 09:09:52.019   285   285 E         : readConfig Cannot open config file /data/vendor/nfc/libnfc-nxpTransit.conf
06-12 09:09:52.019   285   285 D         : readNxpRFConfig-Enter..Reading /system/vendor/libnfc-nxp_RF.conf
06-12 09:09:52.019   285   285 E         : readConfig Cannot open config file /system/vendor/libnfc-nxp_RF.conf
06-12 09:09:52.019   285   285 D NxpHal  : nfc_debug_enabled : 1
06-12 09:09:52.019   285   285 D NxpExtns: find found NXPLOG_NCIHAL_LOGLEVEL=(0x3)
06-12 09:09:52.019   285   285 D NxpExtns: find found NXPLOG_EXTNS_LOGLEVEL=(0x3)
06-12 09:09:52.019   285   285 D NxpExtns: find found NXPLOG_TML_LOGLEVEL=(0x3)
06-12 09:09:52.019   285   285 D NxpExtns: find found NXPLOG_FWDNLD_LOGLEVEL=(0x3)
06-12 09:09:52.019   285   285 D NxpExtns: find found NXPLOG_NCIX_LOGLEVEL=(0x3)
06-12 09:09:52.019   285   285 D NxpExtns: find found NXPLOG_NCIR_LOGLEVEL=(0x3)
06-12 09:09:52.019   285   285 D         : phNxpLog_InitializeLogLevel: global =1, Fwdnld =3, extns =3,                 hal =3, tml =3, ncir =3,                 ncix =3
06-12 09:09:52.019   285   285 D NxpHal  : Entering phNxpNciHal_init_monitor
06-12 09:09:52.019   285   285 D NxpHal  : Returning with SUCCESS
06-12 09:09:52.019   285   285 D EseHalClient: EseAdaptation::Initialize: enter
06-12 09:09:52.019   285   285 D EseHalClient: EseAdaptation::InitializeHalDeviceContext: enter
06-12 09:09:52.019   285   285 D EseHalClient: EseAdaptation::InitializeHalDeviceContext: INxpEse::tryGetService()
06-12 09:09:52.020   244   244 W hwservicemanager: getTransport: Cannot find entry [email protected]::INxpEse/default in either framework or device manifest.
06-12 09:09:52.020   285   285 D EseHalClient: EseAdaptation::InitializeHalDeviceContext: Failed to retrieve the NXP ESE HAL!
06-12 09:09:52.020   285   285 D EseHalClient: EseAdaptation::InitializeHalDeviceContext: exit
06-12 09:09:52.020   285   285 D EseHalClient: EseAdaptation::Initialize: exit
06-12 09:09:52.020   285   285 D NxpExtns: find found NXP_NFC_DEV_NODE=/dev/pn544
06-12 09:09:52.020   285   285 D NxpTml  : Opening port=/dev/pn544
06-12 09:09:52.020   285   285 D NxpTml  : phTmlNfc_i2c_reset(), VEN level 0
06-12 09:09:52.020   285   285 E NxpTml  : phTmlNfc_i2c_reset :failed errno = 0x16
06-12 09:09:52.031   285   285 D NxpTml  : phTmlNfc_i2c_reset(), VEN level 1
06-12 09:09:52.031   285   285 E NxpTml  : phTmlNfc_i2c_reset :failed errno = 0x16
06-12 09:09:52.031   285   285 D         : sem_timedwait() succeeded
06-12 09:09:52.031   285 17986 D NxpTml  : PN54X - Tml Reader Thread Started................
06-12 09:09:52.031   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.031   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.031   285 17989 D NxpHal  : thread started
06-12 09:09:52.032   285 17987 D NxpTml  : PN54X - Tml Writer Thread Started................
06-12 09:09:52.032   285 17987 D NxpTml  : PN54X - Tml Writer Thread Running................
06-12 09:09:52.032   285 17987 D NxpTml  : PN54X - Write requested.....
06-12 09:09:52.032   285 17987 D NxpTml  : PN54X - Invoking I2C Write.....
06-12 09:09:52.033   285 17986 E NxpTml  : _i2c_read() [hdr] errno : 6
06-12 09:09:52.033   285 17986 E NxpTml  : PN54X - Error in I2C Read.....
06-12 09:09:52.034   285 17987 D NxpNciX : len =   4 => 20000100
06-12 09:09:52.034   285 17987 D NxpTml  : PN54X - I2C Write successful.....
06-12 09:09:52.034   285 17987 D NxpTml  : PN54X - Posting Fresh Write message.....
06-12 09:09:52.034   285 17987 D NxpTml  : PN54X - Tml Writer Thread Running................
06-12 09:09:52.034   285 17989 D NxpHal  : write successful status = 0x0
06-12 09:09:52.034   285   285 D NxpHal  : Response timer started
06-12 09:09:52.034   285   285 D NxpHal  : Waiting after ext cmd sent
06-12 09:09:52.063   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.063   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.066   285 17986 D NxpTml  : PN54X - I2C Read successful.....len = 6
06-12 09:09:52.066   285 17986 D NxpTml  : PN54X - Posting read message.....
06-12 09:09:52.066   285 17986 D NxpNciR : len =   6 <= 400003001100
06-12 09:09:52.066   285 17989 D NxpHal  : read successful status = 0x0
06-12 09:09:52.066   285 17989 D NxpHal  : CORE_RESET_RSP NCI1.0
06-12 09:09:52.066   285   285 D NxpHal  : Response timer stopped
06-12 09:09:52.066   285   285 E NxpHal  : nxpncihal_ctrl.ext_cb_data.status 0x0
06-12 09:09:52.066   285   285 D NxpHal  : Checking response
06-12 09:09:52.066   285   285 D         : sem_timedwait() succeeded
06-12 09:09:52.066   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.066   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.066   285 17987 D NxpTml  : PN54X - Write requested.....
06-12 09:09:52.066   285 17987 D NxpTml  : PN54X - Invoking I2C Write.....
06-12 09:09:52.067   285 17986 E NxpTml  : _i2c_read() [hdr] errno : 6
06-12 09:09:52.067   285 17986 E NxpTml  : PN54X - Error in I2C Read.....
06-12 09:09:52.069   285 17987 D NxpNciX : len =   3 => 200100
06-12 09:09:52.069   285 17987 D NxpTml  : PN54X - I2C Write successful.....
06-12 09:09:52.069   285 17987 D NxpTml  : PN54X - Posting Fresh Write message.....
06-12 09:09:52.069   285 17987 D NxpTml  : PN54X - Tml Writer Thread Running................
06-12 09:09:52.069   285 17989 D NxpHal  : write successful status = 0x0
06-12 09:09:52.069   285   285 D NxpHal  : Response timer started
06-12 09:09:52.069   285   285 D NxpHal  : Waiting after ext cmd sent
06-12 09:09:52.097   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.098   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.102   285 17986 D NxpTml  : PN54X - I2C Read successful.....len = 28
06-12 09:09:52.102   285 17986 D NxpTml  : PN54X - Posting read message.....
06-12 09:09:52.102   285 17986 D NxpNciR : len =  28 <= 40011900031E030008000102038081828302D002FF020004881001A0
06-12 09:09:52.103   285 17989 D NxpHal  : read successful status = 0x0
06-12 09:09:52.103   285 17989 D NxpHal  : CORE_INIT_RSP NCI1.0 received !
06-12 09:09:52.103   285 17989 D NxpHal  : NxpNci> FW Version: 10.1.a0
06-12 09:09:52.103   285 17989 D NxpHal  : CORE_INIT_RSP 1 received !
06-12 09:09:52.103   285 17989 D         : getChipType HwVersion : 0x88
06-12 09:09:52.103   285 17989 D         : getChipType NxpNci > Product : PN80T
06-12 09:09:52.103   285 17989 D NxpHal  : NFC_GetFeatureList ()chipType = 8
06-12 09:09:52.103   285   285 D NxpHal  : Response timer stopped
06-12 09:09:52.103   285   285 E NxpHal  : nxpncihal_ctrl.ext_cb_data.status 0x0
06-12 09:09:52.103   285   285 D NxpHal  : Checking response
06-12 09:09:52.103   285   285 D NxpHal  : phNxpNciHal_CheckFwRegFlashRequired() : enter
06-12 09:09:52.103   285   285 D NxpFwDnld: Allocating Mem for Dnld Context..
06-12 09:09:52.103   285   285 D NxpExtns: find found NXP_FW_NAME=libpn547_fw.so
06-12 09:09:52.103   285   285 D NxpFwDnld: @@@/system/vendor/lib/libpn547_fw.so
06-12 09:09:52.103   285   285 E NxpFwDnld: NULL handler : unable to load the library file, specify correct path
06-12 09:09:52.103   285   285 E NxpFwDnld: FW Image Length - ImageInfoLen 0
06-12 09:09:52.103   285   285 E NxpFwDnld: FW Image Info Pointer - pImageInfo 0x0
06-12 09:09:52.103   285   285 E NxpFwDnld: Image extraction Failed - invalid imginfo or imginfolen!!
06-12 09:09:52.103   285   285 E NxpFwDnld: Error loading libpn5xx_fw.so !!!
06-12 09:09:52.103   285   285 E NxpHal  : FW version of the libpn5xx.so binary = 0x0
06-12 09:09:52.103   285   285 E NxpHal  : FW version found on the device = 0x1001a0
06-12 09:09:52.103   285   285 D NxpHal  : FW update not required
06-12 09:09:52.103   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.103   285   285 E NxpFwDnld: Freeing Mem for Dnld Context..
06-12 09:09:52.103   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.103   285   285 D NxpHal  : phNxpNciHal_CheckFwRegFlashRequired() : exit - status = ff
06-12 09:09:52.103   285   285 D NxpHal  : phNxpNciHal_MinOpen(): exit
06-12 09:09:52.103   285   285 E NxpHal  : phNxpNciHal_open Done.
06-12 09:09:52.103   285   285 E NxpHal  : phNxpNciHal_open Exit.
06-12 09:09:52.103   285   285 D [email protected]: Nfc::open(): exit
06-12 09:09:52.104 17963 17984 I libnfc_nci: [INFO:nfc_main.cc(568)] nfc_main_hal_cback event: HAL_NFC_OPEN_CPLT_EVT(0x0), status=0
06-12 09:09:52.104 17963 17983 I libnfc_nci: [INFO:nfc_task.cc(358)] NFC_TASK got NFC_TASK_EVT_TRANSPORT_READY.
06-12 09:09:52.104 17963 17983 I libnfc_nci: [INFO:nfc_main.cc(326)] nfc_set_state 1 (W4_HAL_OPEN)->2 (CORE_INIT)
06-12 09:09:52.104 17963 17983 I libnfc_nci: [INFO:NfcAdaptation.cc(583)] NfcAdaptation::HalWrite
06-12 09:09:52.104   285   285 D NxpExtns: find found MIFARE_READER_ENABLE=(0x1)
06-12 09:09:52.104   285   285 D         : sem_timedwait() succeeded
06-12 09:09:52.104   285 17987 D NxpTml  : PN54X - Write requested.....
06-12 09:09:52.104   285 17987 D NxpTml  : PN54X - Invoking I2C Write.....
06-12 09:09:52.106   285 17987 D NxpNciX : len =   4 => 20000101
06-12 09:09:52.106   285 17987 D NxpTml  : PN54X - I2C Write successful.....
06-12 09:09:52.106   285 17987 D NxpTml  : PN54X - Posting Fresh Write message.....
06-12 09:09:52.106   285 17987 D NxpTml  : PN54X - Tml Writer Thread Running................
06-12 09:09:52.106   285 17986 E NxpTml  : _i2c_read() [hdr] errno : 6
06-12 09:09:52.106   285 17986 E NxpTml  : PN54X - Error in I2C Read.....
06-12 09:09:52.106   285 17989 D NxpHal  : write successful status = 0x0
06-12 09:09:52.136   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.136   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.142   285 17986 D NxpTml  : PN54X - I2C Read successful.....len = 6
06-12 09:09:52.142   285 17986 D NxpTml  : PN54X - Posting read message.....
06-12 09:09:52.143   285 17986 D NxpNciR : len =   6 <= 400003001101
06-12 09:09:52.143   285 17989 D NxpHal  : read successful status = 0x0
06-12 09:09:52.143   285 17989 D NxpHal  : CORE_RESET_RSP NCI1.0
06-12 09:09:52.143 17963 17983 I libnfc_nci: [INFO:nfc_ncif.cc(383)] NFC received rsp gid:0
06-12 09:09:52.144 17963 17983 I libnfc_nci: [INFO:nci_hrcv.cc(62)] nci_proc_core_rsp opcode:0x0
06-12 09:09:52.144 17963 17983 I libnfc_nci: [INFO:nfc_ncif.cc(1365)] CORE_RESET_RSP len :0x3
06-12 09:09:52.144 17963 17983 I libnfc_nci: [INFO:NfcAdaptation.cc(583)] NfcAdaptation::HalWrite
06-12 09:09:52.144   285   285 D NxpExtns: find found MIFARE_READER_ENABLE=(0x1)
06-12 09:09:52.144   285   285 D         : sem_timedwait() succeeded
06-12 09:09:52.144   285 17987 D NxpTml  : PN54X - Write requested.....
06-12 09:09:52.144   285 17987 D NxpTml  : PN54X - Invoking I2C Write.....
06-12 09:09:52.146   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.146   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.146   285 17987 D NxpNciX : len =   3 => 200100
06-12 09:09:52.146   285 17987 D NxpTml  : PN54X - I2C Write successful.....
06-12 09:09:52.146   285 17987 D NxpTml  : PN54X - Posting Fresh Write message.....
06-12 09:09:52.146   285 17987 D NxpTml  : PN54X - Tml Writer Thread Running................
06-12 09:09:52.146   285 17989 D NxpHal  : write successful status = 0x0
06-12 09:09:52.152   285 17986 D NxpTml  : PN54X - I2C Read successful.....len = 28
06-12 09:09:52.153   285 17986 D NxpTml  : PN54X - Posting read message.....
06-12 09:09:52.153   285 17986 D NxpNciR : len =  28 <= 40011900031E030008000102038081828302D002FF020004881001A0
06-12 09:09:52.153   285 17989 D NxpHal  : read successful status = 0x0
06-12 09:09:52.154   285 17989 D NxpHal  : CORE_INIT_RSP NCI1.0 received !
06-12 09:09:52.154   285 17989 D NxpHal  : NxpNci> FW Version: 10.1.a0
06-12 09:09:52.154   285 17989 D NxpHal  : CORE_INIT_RSP 1 received !
06-12 09:09:52.154 17963 17983 I libnfc_nci: [INFO:nfc_ncif.cc(383)] NFC received rsp gid:0
06-12 09:09:52.154 17963 17983 I libnfc_nci: [INFO:nci_hrcv.cc(62)] nci_proc_core_rsp opcode:0x1
06-12 09:09:52.154 17963 17983 I libnfc_nci: [INFO:nfc_ncif.cc(1421)] scbr support: 0x1
06-12 09:09:52.154 17963 17983 I libnfc_nci: [INFO:nfc_main.cc(326)] nfc_set_state 2 (CORE_INIT)->3 (W4_POST_INIT_CPLT)
06-12 09:09:52.154 17963 17983 I libnfc_nci: [INFO:NfcAdaptation.cc(601)] NfcAdaptation::HalCoreInitialized
06-12 09:09:52.155   285   285 D NxpHal  : phNxpNciHal_core_initialized::p_core_init_rsp_params : 64
06-12 09:09:52.155   285   285 D NxpExtns: find found NXP_ACT_PROP_EXTN=/
06-12 09:09:52.155   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.155   285   285 D         : sem_timedwait() succeeded
06-12 09:09:52.155   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.155   285 17987 D NxpTml  : PN54X - Write requested.....
06-12 09:09:52.155   285 17987 D NxpTml  : PN54X - Invoking I2C Write.....
06-12 09:09:52.157   285 17986 E NxpTml  : _i2c_read() [hdr] errno : 6
06-12 09:09:52.157   285 17986 E NxpTml  : PN54X - Error in I2C Read.....
06-12 09:09:52.157   285 17987 D NxpNciX : len =   3 => 2F0200
06-12 09:09:52.157   285 17987 D NxpTml  : PN54X - I2C Write successful.....
06-12 09:09:52.157   285 17987 D NxpTml  : PN54X - Posting Fresh Write message.....
06-12 09:09:52.158   285 17989 D NxpHal  : write successful status = 0x0
06-12 09:09:52.158   285   285 D NxpHal  : Response timer started
06-12 09:09:52.158   285   285 D NxpHal  : Waiting after ext cmd sent
06-12 09:09:52.158   285 17987 D NxpTml  : PN54X - Tml Writer Thread Running................
06-12 09:09:52.187   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.187   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.190   285 17986 D NxpTml  : PN54X - I2C Read successful.....len = 8
06-12 09:09:52.190   285 17986 D NxpTml  : PN54X - Posting read message.....
06-12 09:09:52.191   285 17986 D NxpNciR : len =   8 <= 4F02050000009F97
06-12 09:09:52.191   285 17989 D NxpHal  : read successful status = 0x0
06-12 09:09:52.191   285   285 D NxpHal  : Response timer stopped
06-12 09:09:52.191   285   285 E NxpHal  : nxpncihal_ctrl.ext_cb_data.status 0x0
06-12 09:09:52.191   285   285 D NxpHal  : Checking response
06-12 09:09:52.191   285   285 D         : sem_timedwait() succeeded
06-12 09:09:52.191   285 17987 D NxpTml  : PN54X - Write requested.....
06-12 09:09:52.192   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.192   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.192   285 17987 D NxpTml  : PN54X - Invoking I2C Write.....
06-12 09:09:52.195   285 17987 D NxpNciX : len =   8 => 20020501A0070103
06-12 09:09:52.195   285 17987 D NxpTml  : PN54X - I2C Write successful.....
06-12 09:09:52.195   285 17987 D NxpTml  : PN54X - Posting Fresh Write message.....
06-12 09:09:52.195   285 17989 D NxpHal  : write successful status = 0x0
06-12 09:09:52.195   285   285 D NxpHal  : Response timer started
06-12 09:09:52.195   285   285 D NxpHal  : Waiting after ext cmd sent
06-12 09:09:52.195   285 17987 D NxpTml  : PN54X - Tml Writer Thread Running................
06-12 09:09:52.196   285 17986 E NxpTml  : _i2c_read() [hdr] errno : 6
06-12 09:09:52.197   285 17986 E NxpTml  : PN54X - Error in I2C Read.....
06-12 09:09:52.227   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.227   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.232   285 17986 D NxpTml  : PN54X - I2C Read successful.....len = 5
06-12 09:09:52.232   285 17986 D NxpTml  : PN54X - Posting read message.....
06-12 09:09:52.232   285 17986 D NxpNciR : len =   5 <= 4002020000
06-12 09:09:52.233   285 17989 D NxpHal  : read successful status = 0x0
06-12 09:09:52.233   285 17989 D NxpHal  : phNxpNciHal_print_res_status: response status =STATUS_OK
06-12 09:09:52.233   285   285 D NxpHal  : Response timer stopped
06-12 09:09:52.233   285   285 E NxpHal  : nxpncihal_ctrl.ext_cb_data.status 0x0
06-12 09:09:52.233   285   285 D NxpHal  : Checking response
06-12 09:09:52.233   285   285 E NxpHal  : NAME_NXP_SVDD_SYNC_OFF_DELAY failed
06-12 09:09:52.233   285   285 D NxpHal  : Timeout value
06-12 09:09:52.233   285   285 E         : isModified Unable to open file '/data/vendor/nfc/libnfc-nxpConfigState.bin' - assuming modified
06-12 09:09:52.233   285   285 D NxpHal  : Timeout value - 1
06-12 09:09:52.233   285   285 D NxpHal  : request_EEPROM Enter  request_type : 0x02,  request_mode : 0x01,  bufflen : 0x04
06-12 09:09:52.233   285   285 D         : sem_timedwait() succeeded
06-12 09:09:52.233   285 17987 D NxpTml  : PN54X - Write requested.....
06-12 09:09:52.233   285 17987 D NxpTml  : PN54X - Invoking I2C Write.....
06-12 09:09:52.236   285 17987 D NxpNciX : len =   6 => 20030301A0FC
06-12 09:09:52.236   285 17987 D NxpTml  : PN54X - I2C Write successful.....
06-12 09:09:52.236   285 17987 D NxpTml  : PN54X - Posting Fresh Write message.....
06-12 09:09:52.237   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.237   285 17987 D NxpTml  : PN54X - Tml Writer Thread Running................
06-12 09:09:52.237   285 17989 D NxpHal  : write successful status = 0x0
06-12 09:09:52.237   285   285 D NxpHal  : Response timer started
06-12 09:09:52.237   285   285 D NxpHal  : Waiting after ext cmd sent
06-12 09:09:52.238   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.242   285 17986 D NxpTml  : PN54X - I2C Read successful.....len = 8
06-12 09:09:52.242   285 17986 D NxpTml  : PN54X - Posting read message.....
06-12 09:09:52.244   285 17986 D NxpNciR : len =   8 <= 4003050901A0FC00
06-12 09:09:52.245   285 17989 D NxpHal  : read successful status = 0x0
06-12 09:09:52.245   285 17989 D NxpHal  : phNxpNciHal_print_res_status: response status =STATUS_INVALID_PARAM
06-12 09:09:52.245   285   285 D NxpHal  : Response timer stopped
06-12 09:09:52.245   285   285 E NxpHal  : nxpncihal_ctrl.ext_cb_data.status 0x0
06-12 09:09:52.245   285   285 D NxpHal  : Checking response
06-12 09:09:52.245   285   285 E         : failed to get requested memory address
06-12 09:09:52.245   285   285 E         : isModified Unable to open file '/data/vendor/nfc/libnfc-nxpConfigState.bin' - assuming modified
06-12 09:09:52.245   285   285 D NxpHal  : fw_download_success : 0x00 SetConfigAlways flag : 0x00
06-12 09:09:52.245   285   285 E         : isModified Unable to open file '/data/vendor/nfc/libnfc-nxpConfigState.bin' - assuming modified
06-12 09:09:52.245   285   285 D NxpExtns: find found NXP_SYS_CLK_SRC_SEL=(0x1)
06-12 09:09:52.245   285   285 D NxpExtns: find found NXP_SYS_CLK_FREQ_SEL=(0x0)
06-12 09:09:52.245   285   285 D NxpExtns: find found NXP_SYS_CLOCK_TO_CFG=(0x1)
06-12 09:09:52.245   285   285 D NxpFwDnld: gphNxpNciHal_fw_IoctlCtx.bClkSrcVal = 0x1
06-12 09:09:52.245   285   285 D NxpFwDnld: gphNxpNciHal_fw_IoctlCtx.bClkFreqVal = 0x0
06-12 09:09:52.245   285   285 D NxpFwDnld: gphNxpNciHal_fw_IoctlCtx.bClkFreqVal = 0x1
06-12 09:09:52.245   285   285 E NxpFwDnld: Clock frequency value is wrong in config file, setting it as default
06-12 09:09:52.245   285   285 D         : sem_timedwait() succeeded
06-12 09:09:52.245   285 17987 D NxpTml  : PN54X - Write requested.....
06-12 09:09:52.245   285 17987 D NxpTml  : PN54X - Invoking I2C Write.....
06-12 09:09:52.249   285 17987 D NxpNciX : len =  10 => 20030703A002A003A004
06-12 09:09:52.249   285 17987 D NxpTml  : PN54X - I2C Write successful.....
06-12 09:09:52.249   285 17987 D NxpTml  : PN54X - Posting Fresh Write message.....
06-12 09:09:52.249   285 17987 D NxpTml  : PN54X - Tml Writer Thread Running................
06-12 09:09:52.249   285 17989 D NxpHal  : write successful status = 0x0
06-12 09:09:52.249   285   285 D NxpHal  : Response timer started
06-12 09:09:52.249   285   285 D NxpHal  : Waiting after ext cmd sent
06-12 09:09:52.250   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.250   285 17986 D NxpTml  : PN54X - Invoking I2C Read.....
06-12 09:09:52.255   285 17986 D NxpTml  : PN54X - I2C Read successful.....len = 17
06-12 09:09:52.255   285 17986 D NxpTml  : PN54X - Posting read message.....
06-12 09:09:52.255   285 17986 D NxpNciR : len =  17 <= 40030E0003A0020101A0030108A0040101
06-12 09:09:52.255   285 17989 D NxpHal  : read successful status = 0x0
06-12 09:09:52.255   285 17989 D NxpHal  : phNxpNciHal_print_res_status: response status =STATUS_OK
06-12 09:09:52.256   285   285 D NxpHal  : Response timer stopped
06-12 09:09:52.256   285   285 E NxpHal  : nxpncihal_ctrl.ext_cb_data.status 0x0
06-12 09:09:52.256   285   285 D NxpHal  : Checking response
06-12 09:09:52.256   285   285 D NxpHal  : Setting Clock Source and Frequency
06-12 09:09:52.256   285   285 D NxpExtns: find found NXP_SYS_CLK_SRC_SEL=(0x1)
06-12 09:09:52.256   285   285 D NxpExtns: find found NXP_SYS_CLK_FREQ_SEL=(0x0)
06-12 09:09:52.256   285   285 D NxpHal  : phNxpNciHal_txNfccClockSetCmd : clock source = 1, frequency = 0
06-12 09:09:52.256   285   285 D         : sem_timedwait() succeeded
06-12 09:09:52.256   285 17987 D NxpTml  : PN54X - Write requested.....
06-12 09:09:52.256   285 17987 D NxpTml  : PN54X - Invoking I2C Write.....
06-12 09:09:52.257   285 17986 D NxpTml  : PN54X - Read requested.....
06-12 09:09:52.258   285 17987 D NxpNciX : len =   8 => 20020501A0030108
06-12 09:09:52.258   285 17987 D NxpTml  : PN54X - I2C Write successful.....
06-12 09:09:52.258   285 17987 D NxpTml  : PN54X - Posting Fresh Write message.....
06-12 09:09:52.258   285 17987 D NxpTml  : PN54X - Tml Writer Thread Running................
06-12 09:09:52.258   285 17989 D NxpHal  : write successful status = 0x0
06-12 09:09:52.259   285   285 D NxpHal  : Response timer started
06-12 09:09:52.259   285   285 D NxpHal  : Waiting after ext cmd sent

0 件の賞賛
返信
6 返答(返信)

4,254件の閲覧回数
nanbaolin
Contributor I

Hi,All:

    this issue had solved,it was casued by HW issue. IRQ always high.

thanks!

0 件の賞賛
返信

4,254件の閲覧回数
sivasu4098
Contributor III

     I had gone through the Application note. drivers are built for pn544. Then in device tree , I have to assign either pn544 or pn7150. I s this below driver is suitable for PN7150 Chip. Please confirm it.

GitHub - NXPNFCLinux/nxp-pn5xx: NXP's NFC Open Source Kernel mode driver 

0 件の賞賛
返信

4,254件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

You can refer this :

https://www.nxp.com/docs/en/application-note/AN11697.pdf 

In 3.1.2.3, there is example for device tree setting

0 件の賞賛
返信

4,254件の閲覧回数
sivasu4098
Contributor III

for kernel driver in PN7150 porting you are using which one among pn544 or p547 or pn548. Kindly suggest the part number

0 件の賞賛
返信

4,254件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

4,254件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信