PN7150 or CLRC663?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 or CLRC663?

2,426件の閲覧回数
kevin-swiftlabs
Contributor I

Hi, I'm designing an access control product that needs to support all MIFARE and ISO 15693 cards. I am already using an ARM Cortex-M3 part for some other features of the product and need to decide between using the CLRC663plus and the PN7150. It seems like the PN7150 is a no-brainer since it has all the library firmware already included thus saving on my MCU's flash, RAM and processing as well. Is there any disadvantage to using the PN7150 instead of the CLRC part that I'm not seeing? Even the pricing is better on the PN7150.

Thanks!

タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,180件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Which is your target distance? Are you looking to support any other ISO ? 

Best Regards 

Estephania 

0 件の賞賛
返信

2,180件の閲覧回数
kevin-swiftlabs
Contributor I

The two parts support the same standards according to their datasheet so I don't think there is any differentiation there. The target distance is contact to 10cm. Is there a range performance difference between the two parts?

Thanks

Kevin

0 件の賞賛
返信