PN7150 or CLRC663?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 or CLRC663?

2,423 Views
kevin-swiftlabs
Contributor I

Hi, I'm designing an access control product that needs to support all MIFARE and ISO 15693 cards. I am already using an ARM Cortex-M3 part for some other features of the product and need to decide between using the CLRC663plus and the PN7150. It seems like the PN7150 is a no-brainer since it has all the library firmware already included thus saving on my MCU's flash, RAM and processing as well. Is there any disadvantage to using the PN7150 instead of the CLRC part that I'm not seeing? Even the pricing is better on the PN7150.

Thanks!

Tags (3)
0 Kudos
Reply
2 Replies

2,177 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Which is your target distance? Are you looking to support any other ISO ? 

Best Regards 

Estephania 

0 Kudos
Reply

2,177 Views
kevin-swiftlabs
Contributor I

The two parts support the same standards according to their datasheet so I don't think there is any differentiation there. The target distance is contact to 10cm. Is there a range performance difference between the two parts?

Thanks

Kevin

0 Kudos
Reply