PN7150 nfcDemoApp poll Crash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 nfcDemoApp poll Crash

905 Views
ethan_dang1
Contributor III

I use Raspberry 3B & OM5579/PN7150RPI run the demo "nfcDemoApp poll " follow Easy set-up of NFC on Raspberry Pi - NXP Community

Usually works normally,But when I put 2 MIFARE Classic cards into the field at the same time many times in a row, it crashed.

(

it’s ok when put 2 NTAG213 cards into the field at the same time many times in a row;

it’s ok when put only one MIFARE Classic card into the field at the same time many times in a row;

)

Why? There are logs here, please help analyze them ,Thanks!

0 Kudos
Reply
2 Replies

887 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @ethan_dang1 

Thanks for sharing and contacting us. Based on your description I'd like to know why do you put two mifare classic cards on the field at the same and does your application scenario have to be like this? I want to know this because I need to make sure if the Demo supports this application scenario.

To update this case, you may reply by email.
To provide confidential information or attachments, you may add that online.

Please login to our NXP technical support portal:
https://support.nxp.com/s/case/5002p00002s4gPIAAY

The portal allows access to the full details of the case, including the previous communication.

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

Best regards,
Kelly
Technical Support
NXP Semiconductor

0 Kudos
Reply

881 Views
ethan_dang1
Contributor III

Hi Kelly @KaiLi 

Put two mifare classic cards on the field at the same because it happens sometimes(.e.g Multiple cards in the wallet,just put wallet directly into the field)

0 Kudos
Reply