PN7150 Output power?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 Output power?

1,990 Views
erkka_laine
Contributor I

Hi, I'm looking for PN7150 output power for the type approvals. I can't find this information of the datasheet.

Labels (1)
0 Kudos
Reply
1 Reply

1,797 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes, there is  not the type value for it. One may refer to the below information.

The PN7150 has also a programmable transmitter output power from 3.0V to 4.75V even if not given in dBm.

 PN7150 can have TVDD adjustable and depending on the Impedance Tuning also the Current consumption is different.

Example: if a Tuning at 20ohm is done the IC can drive approx 1Watt of Output power to the Antenna (TVDD = 5V and ITVDD = 0.2A).

Hava a nice day.

Best regards

0 Kudos
Reply